Baud_Rate

Baud_Rate

Address: 16569 (40B9H)
Type: WORD
Access:

Read or Read/Write

Unit: mV
Range: 0 to 7 (Modbus: 0 = 115.2k, 1= 57.6k, 2 = 38.4k, 3 = 19.2k, 4 = 9.6k, 5 = 4.8k, 6 = 2.4k, 7 = 1.2)
Default Value:

--

Store Supported:

Yes

Description:

This object contains the drive's Node Id. On drives with dip-switches/rotoswitches the object is read-only. On drives without dip-switches/rotoswitches this object can be changed using the KOLLMORGEN Space or following the procedure explained at §10.1.2.

Notes:

--